AXIS#.MOTOR.NAME

Description

This parameter is the motor name.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

20 chars

Default Value

empty

Data Type

String

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.NAME

500bh

21h

String(20)

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6237

1

6237 (0x185d)

AXIS1.MOTOR.NAME

String

Read Only

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MOTOR.NAME

6237

String

Read Only

-